Sabre Smart Devices MMC Socket

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre Smart Devices MMC Socket

Jump to solution
1,576 Views
atillametetured
Contributor V

Hello

Quick question is, why doesnt the SD Card socket (or MMC socket) on the Sabre Smart Devices doesnt have pull up resistors on data lines. Isnt this mandatory for the SD card specification. Or is it because it is actually a MMC socket? Please enlighten me on the subject.

Thanks,

Mete

Labels (2)
0 Kudos
Reply
1 Solution
1,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

i.MX6 pads have internal pull-up resistors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,527 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

i.MX6 pads have internal pull-up resistors.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------