Hi,all
I test DDR by uboot cmd mtest, And I find on FSL mx6dl, the uboot image will load start from 0x1780 0000, but when I test DDR addr range from 0x1780 0000 to 0x1790 0000, it can test pass,why not crash? I cannot understand, so please help~Thank you ~
Hello,
U-boot is not intended to test memory carefully.
Please use the Stress test instead.
i.MX6/7 DDR Stress Test Tool V2.40
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Yuri,
Now I find a bug. the DDR that I porting have serious problem in memory. But it cannot be detected by your DDR stress tool, Because all test is pass,
But I test by uboot cmd mtest, it is error. So, Could you help me ? FAE cannot answer me, It's a very serious problem.
Does U-boot performs the same DRAM initialization (via DCD) as
Stress tool initialization script ?
Regards,
Yuri.
Yes, Uboot version is 2014.04
And the script can work well on Android 4.2, but Android 5.0 cannot
So its amazing.Please help,thank you ~
Hello,
let me look at Android 5.0 (U-boot) DDR initialization
and the DDR init script of the Stress tester.
Regards,
Yuri.
Hi Yuri,
I think this problem is complicated and is valued for FSL, so if you can call me, that's nice. Because pushing message one by one is inefficient.
Thank you~
I created Case:00066815 for further discussion.
You may send me all needed docs (for analyzing) via this SR,
but I have no Your e-mail. Please let me know it.
My email : yuri.muhin@nxp.com
Regards,
Yuri.