Sabre Board for Smart Devices question?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabre Board for Smart Devices question?

ソリューションへジャンプ
2,906件の閲覧回数
sparkyee
Contributor I


Hi,

    I just recieved my Sabre Board for Smart Devices. I have gotten the

board to boot to a serial console OK. I ahve also hooked up a HDMI

monitor and can see ANDROID booting up to a start screen with a

clock and lock symbol showing. I have tried to get a mouse and/or keyboard

to work on the other USBOTG port but they don't see to have power. I

am trying to unlock the ANDROID screen to see other APPS.  I also

tried putting a mouse on the Debug USB/serial emulator port with no

success. How do I power up these peripherals??

Thanks a Lot!

Larry

ラベル(2)
0 件の賞賛
返信
1 解決策
2,601件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Larry,

     By default, USB OTG works as device, It's power is not opened. If you want it to work as a host, you do a little modification in BSP source code. open linux/arch/arm/mach-mx6/board-mx6q_sabresd.c,and find function "static void __init imx6q_sabresd_init_usb(void)", in this function, open USB OTG POWER. see following:

static void __init imx6q_sabresd_init_usb(void)

{

....

//gpio_direction_output(SABRESD_USB_OTG_PWR, 0);

gpio_direction_output(SABRESD_USB_OTG_PWR, 1);

...

}

then recompile linux kernel and burn it into iNAND FLASH or SD card , boot your board, USB OTG can be used as HOST, your mouse can be used.

Reards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,231件の閲覧回数
ybradid
Contributor I

hello i've just received my sabre board  kit , and i plugged a cbales nothing displayed on screen ,nor on termina putty , what to do ? 

0 件の賞賛
返信
2,601件の閲覧回数
Yuri
NXP Employee
NXP Employee

I tried to connect a USB mouse on the SDP with the recent Android (13.4.1) demo image - it works.

2,601件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Yuri & Larry,

     The BSP I checked is linux(L3.0_1.1.0_121218 Version),So Thank you for your supplying status of OTG on android.

Regards,

Weidong

2,602件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Larry,

     By default, USB OTG works as device, It's power is not opened. If you want it to work as a host, you do a little modification in BSP source code. open linux/arch/arm/mach-mx6/board-mx6q_sabresd.c,and find function "static void __init imx6q_sabresd_init_usb(void)", in this function, open USB OTG POWER. see following:

static void __init imx6q_sabresd_init_usb(void)

{

....

//gpio_direction_output(SABRESD_USB_OTG_PWR, 0);

gpio_direction_output(SABRESD_USB_OTG_PWR, 1);

...

}

then recompile linux kernel and burn it into iNAND FLASH or SD card , boot your board, USB OTG can be used as HOST, your mouse can be used.

Reards,

Weidong

0 件の賞賛
返信