Sabre Board for Smart Devices question?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sabre Board for Smart Devices question?

跳至解决方案
4,284 次查看
sparkyee
Contributor I


Hi,

    I just recieved my Sabre Board for Smart Devices. I have gotten the

board to boot to a serial console OK. I ahve also hooked up a HDMI

monitor and can see ANDROID booting up to a start screen with a

clock and lock symbol showing. I have tried to get a mouse and/or keyboard

to work on the other USBOTG port but they don't see to have power. I

am trying to unlock the ANDROID screen to see other APPS.  I also

tried putting a mouse on the Debug USB/serial emulator port with no

success. How do I power up these peripherals??

Thanks a Lot!

Larry

标签 (2)
0 项奖励
回复
1 解答
3,979 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Larry,

     By default, USB OTG works as device, It's power is not opened. If you want it to work as a host, you do a little modification in BSP source code. open linux/arch/arm/mach-mx6/board-mx6q_sabresd.c,and find function "static void __init imx6q_sabresd_init_usb(void)", in this function, open USB OTG POWER. see following:

static void __init imx6q_sabresd_init_usb(void)

{

....

//gpio_direction_output(SABRESD_USB_OTG_PWR, 0);

gpio_direction_output(SABRESD_USB_OTG_PWR, 1);

...

}

then recompile linux kernel and burn it into iNAND FLASH or SD card , boot your board, USB OTG can be used as HOST, your mouse can be used.

Reards,

Weidong

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,609 次查看
ybradid
Contributor I

hello i've just received my sabre board  kit , and i plugged a cbales nothing displayed on screen ,nor on termina putty , what to do ? 

0 项奖励
回复
3,979 次查看
Yuri
NXP Employee
NXP Employee

I tried to connect a USB mouse on the SDP with the recent Android (13.4.1) demo image - it works.

3,979 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Yuri & Larry,

     The BSP I checked is linux(L3.0_1.1.0_121218 Version),So Thank you for your supplying status of OTG on android.

Regards,

Weidong

3,980 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Larry,

     By default, USB OTG works as device, It's power is not opened. If you want it to work as a host, you do a little modification in BSP source code. open linux/arch/arm/mach-mx6/board-mx6q_sabresd.c,and find function "static void __init imx6q_sabresd_init_usb(void)", in this function, open USB OTG POWER. see following:

static void __init imx6q_sabresd_init_usb(void)

{

....

//gpio_direction_output(SABRESD_USB_OTG_PWR, 0);

gpio_direction_output(SABRESD_USB_OTG_PWR, 1);

...

}

then recompile linux kernel and burn it into iNAND FLASH or SD card , boot your board, USB OTG can be used as HOST, your mouse can be used.

Reards,

Weidong

0 项奖励
回复