SXGA resolution on VGA output not working in Kernels > 2.6.35.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SXGA resolution on VGA output not working in Kernels > 2.6.35.3

1,456 次查看
KaiMayer
Contributor I

Hi!

I've compiled and tried many kernels over the last days and no kernel seems to support 1280x1024 resolution setting for the VGA connector on the i.MX53 QSB.

Only the original 2.6.35.3 kernel branch for IMX seems to support this resolution.

VGA output works well, but the kernel ignores the u-boot settings for the VGA output and permanently switches to 1024x768@60.

Has someone tried and sucessfully got SXGA on VGA working with newer self-compiled kernels (e.g. 3.6.39) ?

 

Kind regards

Kai

标记 (1)
0 项奖励
回复
2 回复数

1,285 次查看
KaiMayer
Contributor I

Kernel says on bootup:

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver vga
_regulator_get: get() with no identifier
imx-ipuv3 imx-ipuv3.0: Channel already disabled 9
imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 9
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
imx-ipuv3 imx-ipuv3.0: Channel already disabled 10
imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 10
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver vga
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver failed with -22

So driver for fb1 fails to register :(

Kind regards

Kai

0 项奖励
回复

1,285 次查看
daiane_angolini
NXP Employee
NXP Employee
0 项奖励
回复