SXGA output from HDMI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SXGA output from HDMI

1,528 次查看
eishishibusawa
Contributor III

Dear Sir

 

Customer is considering a system using i.MX6DL and L4.9.88_2.0.0.

Please tell me how to output from HDMI of i.MX6DL with SXGA (1280 x 1024 @ 60fps).

 

Q1.

Is it able to output SXGA image from HDMI using i.MX6DL and L4.9.88_2.0.0?

 

Q2.

If possible, how can I do it?

 

Best Regards,

Eishi SHIBUSAWA

 

标签 (4)
0 项奖励
回复
1 回复

1,375 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

>Q1.Is it able to output SXGA image from HDMI using i.MX6DL and L4.9.88_2.0.0?

sorry, formally 1280 x 1024 resolution is not supported by HDMI module according to

Table 33-3. Video Modes i.MX6DQ Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

 

>Q2.If possible, how can I do it?

one can try community efforts (solutions formally not supported by nxp) :

Bugs fixed in Linux imx6 HDMI driver 

i.MX6 HDMI audio - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复