SW JPEG Codec for i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SW JPEG Codec for i.MX6UL

跳至解决方案
1,409 次查看
yuuki
Senior Contributor II

Dear all,

We refer to i.MX_Linux_Rerease_Notes for LinuxBSP of i.MX6UL.

(fsl-yocto-L3.14.52_1.1.0-ga.tar.gz)

In Image codec specification of this document, Encode/Decode of the JPEG is performed by software.

JPEG for i.MX6UL.png

Would you tell me the maximum size that i.MX6UL can support?

Can this support MJPEG, too?

If yes, would you tell me maximum size and fps ?

Best Regards,

Yuuki

标签 (2)
0 项奖励
回复
1 解答
1,210 次查看
b36401
NXP Employee
NXP Employee

Please note that i.MX6 UL processor has no Image Processing Unit

and all image processing should be performed in the software.

So there are no any special limitations to image size.

As for MJPEG it should be en-/decoded in the software too.

So there is no any special limitations too.

And we have no FPS estimations regarding these codecs.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------                                                            

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,211 次查看
b36401
NXP Employee
NXP Employee

Please note that i.MX6 UL processor has no Image Processing Unit

and all image processing should be performed in the software.

So there are no any special limitations to image size.

As for MJPEG it should be en-/decoded in the software too.

So there is no any special limitations too.

And we have no FPS estimations regarding these codecs.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------                                                            

0 项奖励
回复