SW JPEG Codec for i.MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SW JPEG Codec for i.MX6UL

ソリューションへジャンプ
2,137件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We refer to i.MX_Linux_Rerease_Notes for LinuxBSP of i.MX6UL.

(fsl-yocto-L3.14.52_1.1.0-ga.tar.gz)

In Image codec specification of this document, Encode/Decode of the JPEG is performed by software.

JPEG for i.MX6UL.png

Would you tell me the maximum size that i.MX6UL can support?

Can this support MJPEG, too?

If yes, would you tell me maximum size and fps ?

Best Regards,

Yuuki

ラベル(2)
0 件の賞賛
返信
1 解決策
1,938件の閲覧回数
b36401
NXP Employee
NXP Employee

Please note that i.MX6 UL processor has no Image Processing Unit

and all image processing should be performed in the software.

So there are no any special limitations to image size.

As for MJPEG it should be en-/decoded in the software too.

So there is no any special limitations too.

And we have no FPS estimations regarding these codecs.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------                                                            

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,939件の閲覧回数
b36401
NXP Employee
NXP Employee

Please note that i.MX6 UL processor has no Image Processing Unit

and all image processing should be performed in the software.

So there are no any special limitations to image size.

As for MJPEG it should be en-/decoded in the software too.

So there is no any special limitations too.

And we have no FPS estimations regarding these codecs.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------                                                            

0 件の賞賛
返信