SPI port via the Audio Code header

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI port via the Audio Code header

1,488 次查看
Don_ng
Contributor I

Has anyone ever tried to run a SPI device off the Audio Code Header on the iMX 25 PDK Personality board?  I have a chip with an SPI interface, but it has a few quirks.  I need to experiment with the chip first to decide if "so broke" we have to bit-bang it or if the SPI interface on the chip is functional enough to run over SPI.  That seems like the easiest access point to an SPI port, but curious if anyone else has tried it.  Or if there is a better solution I'm not seeing ....

标签 (1)
0 项奖励
回复
2 回复数

1,405 次查看
ZaheerAhmad
Contributor II

Yes, I have developed iMX25 PDK 3stack SPI driver for Nucleus Plus RTOS and tested it with the pin outs available at audio. jac.

0 项奖励
回复

1,405 次查看
hosnihosni
Contributor I

Hi

i'm working with nucleus ready start on the spi ,actualy i'am trying to make something  work with the lwspi driver ,but the problem is that i don't really know how to start ,and the nucleus approach is new to me .

0 项奖励
回复