SPI port via the Audio Code header

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI port via the Audio Code header

2,156件の閲覧回数
Don_ng
Fresh Out Contributor

Has anyone ever tried to run a SPI device off the Audio Code Header on the iMX 25 PDK Personality board?  I have a chip with an SPI interface, but it has a few quirks.  I need to experiment with the chip first to decide if "so broke" we have to bit-bang it or if the SPI interface on the chip is functional enough to run over SPI.  That seems like the easiest access point to an SPI port, but curious if anyone else has tried it.  Or if there is a better solution I'm not seeing ....

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,073件の閲覧回数
ZaheerAhmad
Contributor II

Yes, I have developed iMX25 PDK 3stack SPI driver for Nucleus Plus RTOS and tested it with the pin outs available at audio. jac.

0 件の賞賛
返信

2,073件の閲覧回数
hosnihosni
Contributor I

Hi

i'm working with nucleus ready start on the spi ,actualy i'am trying to make something  work with the lwspi driver ,but the problem is that i don't really know how to start ,and the nucleus approach is new to me .

0 件の賞賛
返信