SPI communication on MCIMX8M-EVKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI communication on MCIMX8M-EVKB

Jump to solution
2,479 Views
neo2
Contributor III

Dear NXP

I have an MCIMX8M-EVKB board.

Is there a location where SPI is available to connect to another NXP board?

The only header I see is J801 but that only seems to have a I2C interface.

Or is it is not possible to connect the MCIMX8M board as there are no spare SPI headers or points to connect the 4 wires?

Regards

Lee.

0 Kudos
Reply
1 Solution
2,444 Views
Juan-Rodarte
NXP Employee
NXP Employee

Hi Neo,

No, this board does not have an SPI port. yes you could the ethernet.

Best Regards.

Diego.

View solution in original post

0 Kudos
Reply
2 Replies
2,464 Views
neo2
Contributor III

Replying to my own question.

Based on what I seen on the schematic I don't see a suitable point SPI interfaces 

1. the ECSPI interfaces are being used up by the board itself for it's own chips

2. the QSPI interface is just for Flash rather than a generic SPI. I don't see MOSI and MISO on that interface.

I'll probably used the Ethernet interface instead.

0 Kudos
Reply
2,445 Views
Juan-Rodarte
NXP Employee
NXP Employee

Hi Neo,

No, this board does not have an SPI port. yes you could the ethernet.

Best Regards.

Diego.

0 Kudos
Reply