SPI communication on MCIMX8M-EVKB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI communication on MCIMX8M-EVKB

ソリューションへジャンプ
2,483件の閲覧回数
neo2
Contributor III

Dear NXP

I have an MCIMX8M-EVKB board.

Is there a location where SPI is available to connect to another NXP board?

The only header I see is J801 but that only seems to have a I2C interface.

Or is it is not possible to connect the MCIMX8M board as there are no spare SPI headers or points to connect the 4 wires?

Regards

Lee.

0 件の賞賛
返信
1 解決策
2,448件の閲覧回数
Juan-Rodarte
NXP Employee
NXP Employee

Hi Neo,

No, this board does not have an SPI port. yes you could the ethernet.

Best Regards.

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,468件の閲覧回数
neo2
Contributor III

Replying to my own question.

Based on what I seen on the schematic I don't see a suitable point SPI interfaces 

1. the ECSPI interfaces are being used up by the board itself for it's own chips

2. the QSPI interface is just for Flash rather than a generic SPI. I don't see MOSI and MISO on that interface.

I'll probably used the Ethernet interface instead.

0 件の賞賛
返信
2,449件の閲覧回数
Juan-Rodarte
NXP Employee
NXP Employee

Hi Neo,

No, this board does not have an SPI port. yes you could the ethernet.

Best Regards.

Diego.

0 件の賞賛
返信