SPI Flashing for IMX6ULL based processor SOM using uuu tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Flashing for IMX6ULL based processor SOM using uuu tool

ソリューションへジャンプ
1,186件の閲覧回数
Embedded-world
Contributor IV

Dear Experts,

I'm working with a custom EVB featuring an i.MX6ULL (MCIMX6Y2CVM08AB) processor. I'm attempting to store the image in the SPI flash (NOR) on our custom board. Physically, the micro USB port is connected from the board to a PC (Linux host machine) and powered up. I've configured the boot mode switches as serial down loader on the EVB.

After connecting to the PC, I've tried multiple commands for flashing the SPI, but I keep encountering the following error:

--------------------------------------------------------------------------------------------------------------------------------------------

uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193

Wait for Known USB Device Appear...
Error: fail open file: >qspi_bootloader

---------------------------------------------------------------------------------------------------------------------------------------------

Could someone properly guide me on How to store the built images (u-boot.imx) file into the SPI NOR flash using the uuu tool and boot from the SPI flash method on the custom EVB board?

 

--------------------------------------------------------------------------------------------------------------------------------------------------------------

Also i refereed the : uuu tool https://www.google.com/url?sa=t&source=web&rct=j&opi=89978449&url=https://community.nxp.com/pwmxy876...

--------------------------------------------------------------------------------------------------------------------------------------------------------------

Thanks in advance.

 

Regards,

Ravikumar

0 件の賞賛
返信
1 解決策
1,126件の閲覧回数
Embedded-world
Contributor IV

Hi @JosephAtNXP 

Thanks for your response.

I tried multiple times to flash QSPI, and finally, I succeeded by using the command "sudo uuu -b qspi <Generated u-boot.imx image>" from uuu user guide.pdf. If I need any further help, I'll definitely get back to you.

 

 

Thanks & Regards,

Ravikumar

元の投稿で解決策を見る

2 返答(返信)
1,127件の閲覧回数
Embedded-world
Contributor IV

Hi @JosephAtNXP 

Thanks for your response.

I tried multiple times to flash QSPI, and finally, I succeeded by using the command "sudo uuu -b qspi <Generated u-boot.imx image>" from uuu user guide.pdf. If I need any further help, I'll definitely get back to you.

 

 

Thanks & Regards,

Ravikumar

1,145件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

What is the filename for the imx-boot binary, you are referencing qspi_bootloader from your command which is not found.

Could you send the logs of uuu recognizing the serial download device, the flashing attempt and that the file exist is current folder?

Regards

0 件の賞賛
返信