SPDIF maximum sampling rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPDIF maximum sampling rate

Jump to solution
1,863 Views
yoshida_satoru
Contributor II

I'm planning to use the SPDIF of the i.MX RT 1060.
What is the maximum sample rate that SPDIF can input and output?
Is 192kHz correct?

Tags (2)
0 Kudos
Reply
1 Solution
1,815 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Correct, up to 192kHz.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
1 Reply
1,816 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Correct, up to 192kHz.

Best regards,
Omar

0 Kudos
Reply