SPD command DCD write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPD command DCD write

1,276 次查看
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you how to set(change) the register value after POR in Serial Download.

I think that it is able to execute with the SPD command DCD write.

SPD command DCD write will be in SPD file.

 

Customer is using the LTIB 3.0.35 for i.MX6.

Q1.

Where is the SPD command file?

 

Best Regards,

 

标签 (2)
0 项奖励
回复
1 回复

1,194 次查看
Yuri
NXP Employee
NXP Employee

Hello

  Please refer to Chapter 1 (Porting U-Boot from an i.MX 6Dual/6Quad Reference
Board to an i.MX 6Dual/6Quad Custom Board) of the BSP Porting Guide in BSP docs.
In particular, please use section "Changing the DCD Table for i.MX 6 DDR3 Initialization".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复