SPD command DCD write

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPD command DCD write

1,318件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you how to set(change) the register value after POR in Serial Download.

I think that it is able to execute with the SPD command DCD write.

SPD command DCD write will be in SPD file.

 

Customer is using the LTIB 3.0.35 for i.MX6.

Q1.

Where is the SPD command file?

 

Best Regards,

 

ラベル(2)
0 件の賞賛
返信
1 返信

1,236件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  Please refer to Chapter 1 (Porting U-Boot from an i.MX 6Dual/6Quad Reference
Board to an i.MX 6Dual/6Quad Custom Board) of the BSP Porting Guide in BSP docs.
In particular, please use section "Changing the DCD Table for i.MX 6 DDR3 Initialization".

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信