SNVS_LPCR[TOP] bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SNVS_LPCR[TOP] bit

1,763件の閲覧回数
julesg
Contributor I

Hello,

We have a custom board which is based on the sabreSmart eval board (http://community.qnx.com/sf/wiki/do/viewPage/projects.bsp/wiki/FreescaleImx6QSabreSmart). I am trying to power off the system from software but not having much luck. I have verified that the DP_EN bit is enabled but when I write 1 to the TOP bit, nothing seems to happen. The ref manual doesn't seem clear to me how this is supposed to work however it does say that this bit is supposed to power off the system. Please advise. Thanks.

Note: I am using QNX

ラベル(2)
0 件の賞賛
返信
1 返信

1,517件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jules

one can look at patch below showing TOP bit usage

Q&A: How is mx6 PMIC_ON_REQ under SW control?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信