SNVS_LPCR[TOP] bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SNVS_LPCR[TOP] bit

1,218 Views
julesg
Contributor I

Hello,

We have a custom board which is based on the sabreSmart eval board (http://community.qnx.com/sf/wiki/do/viewPage/projects.bsp/wiki/FreescaleImx6QSabreSmart). I am trying to power off the system from software but not having much luck. I have verified that the DP_EN bit is enabled but when I write 1 to the TOP bit, nothing seems to happen. The ref manual doesn't seem clear to me how this is supposed to work however it does say that this bit is supposed to power off the system. Please advise. Thanks.

Note: I am using QNX

Labels (2)
0 Kudos
Reply
1 Reply

972 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jules

one can look at patch below showing TOP bit usage

Q&A: How is mx6 PMIC_ON_REQ under SW control?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply