SDK2.2_iMX6UL_WIN for new create project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK2.2_iMX6UL_WIN for new create project

1,765件の閲覧回数
kyleyang
Contributor IV

Hi sirs,

I had download the SDK2.2_iMX6UL_WIN and try to create a new stand alone freeRTOS project code.

I try to use "KSDK-Project-Generator" tool to create or clone a project code, but not works.

Is there any recommend method for me to solve this issue?

thanks.

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,524件の閲覧回数
art
NXP Employee
NXP Employee

Please refer to the attached document. It is also included in the SDK package.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,524件の閲覧回数
kyleyang
Contributor IV

Hi Artur

Thanks.

I had check that before, but did not match what I need.

I want to new create a stand alone project code, is there any way to achieve?

0 件の賞賛
返信