SDK2.2_iMX6UL_WIN for new create project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK2.2_iMX6UL_WIN for new create project

1,797 Views
kyleyang
Contributor IV

Hi sirs,

I had download the SDK2.2_iMX6UL_WIN and try to create a new stand alone freeRTOS project code.

I try to use "KSDK-Project-Generator" tool to create or clone a project code, but not works.

Is there any recommend method for me to solve this issue?

thanks.

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

1,556 Views
art
NXP Employee
NXP Employee

Please refer to the attached document. It is also included in the SDK package.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,556 Views
kyleyang
Contributor IV

Hi Artur

Thanks.

I had check that before, but did not match what I need.

I want to new create a stand alone project code, is there any way to achieve?

0 Kudos
Reply