SDK 2.7.0 - broken?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDK 2.7.0 - broken?

跳至解决方案
4,426 次查看
tamir_michael
Contributor IV

Hello,

I am running MCUXpresso v11.0.1 on Linux, with SDK_2.X_EVK-MIMXRT1064 installed.

However, none of the newly generated SDKs v2.7.0 can be installed - they all report 

"java.lang.Exception: java.io.IOException: Unable to find valid manifest files in SDK".

Removing the SDK I have installed, restarting the IDE and attempting to add the new SDK as the first and only one _also_ fails.

Please fix ASAP !

标记 (2)
0 项奖励
回复
1 解答
4,252 次查看
tamir_michael
Contributor IV

The problem was that SDK 2.7.0 only works with IDE 11.1.0 and better.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
4,252 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Tamir Michael,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I was wondering if you can share the screenshot of the error message, as I haven't encountered the similar error you described.

pastedImage_1.png

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
4,252 次查看
tamir_michael
Contributor IV

pastedImage_1.png

This problem is also reported if there are no other SDKs present (the ones that are present are 2.6.x for RT1060 and 1064).

0 项奖励
回复
4,252 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Tamir Michael,

Thanks for your reply.
It seems a bit weird, whether you can replicate the phenomenon on other PCs.

Have a great day,

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
4,252 次查看
tamir_michael
Contributor IV

Hi,

A colleague will be installing MCUXpresso as well soon - hopefully I will then be able to provide more information. Thanks.

0 项奖励
回复
4,253 次查看
tamir_michael
Contributor IV

The problem was that SDK 2.7.0 only works with IDE 11.1.0 and better.

0 项奖励
回复