SDIO card enumeration problem on Android marshamallow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDIO card enumeration problem on Android marshamallow

3,844件の閲覧回数
susangracerapak
Contributor II

Hi,

I am working on porting my WIFI driver on Android marshmallow for Sabresd board. I have ported for USB successfully.for SDIO,the enumeration is failed.I have observed that , by default only BCMDHD module can used here.
How to use my own SDIO card ?

Can anyone help me ?

Regards

Susan

0 件の賞賛
返信
1 返信

3,682件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Susan

you should obtain driver (compatible with used linux kernel version) from

vendor of custom wifi sdio card and include it in linux image, BCMDHD module

can be removed from image using attached Linux Manual sect.4.12.2.3 Menu Configuration Options.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信