SDHC1 emmc boot for imx8mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDHC1 emmc boot for imx8mini

Jump to solution
2,170 Views
nxf65233
NXP Employee
NXP Employee

Hello everyone,

When designing imX8Mini hardware, customers will switch emmc from SDHC3 to SDHC1.
I have some questions about the following part of the imx8M Mini Reference Manual. The RM contains the following information:

 
 
 

8fe10e5135f7dbbd1e10e22980cf107.png

ECSPI2 and ECSPI1 in the reference manual are not configured with alt2 MUX.SD3_DATA could not be queried in the manual.

I have some questions about the description of this chapter.

I have some questions about whether emmc can be boot with SDHC1 in imx8Mini.
Whether emmc can be boot in SDHC1. 

How should I configure emmc if it can be boot from SDHC1?


Thank you for your attention



0 Kudos
Reply
1 Solution
2,115 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I have discussed with our colleague, and he write a document , You can see the document create by our engineer today https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enabling-uSDHC1-of-i-MX8MM-Based-On-L5-4...

View solution in original post

0 Kudos
Reply
4 Replies
2,144 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The emmc can be boot in SDHC1. You need to configure the SDHC1 clock in u-boot. The details on the SDHC1 configuration I will share to you later.

0 Kudos
Reply
2,135 Views
nxf65233
NXP Employee
NXP Employee

Thank you, look forward to the information you will share

0 Kudos
Reply
2,116 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I have discussed with our colleague, and he write a document , You can see the document create by our engineer today https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enabling-uSDHC1-of-i-MX8MM-Based-On-L5-4...

0 Kudos
Reply
2,108 Views
nxf65233
NXP Employee
NXP Employee

Thanks For your Reply.

0 Kudos
Reply