SCU ROM boot time on IMX8QXP MEK board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCU ROM boot time on IMX8QXP MEK board.

2,897件の閲覧回数
tiebing_guo
Contributor I

Dear Sirs

We are using android_p9.0.0_1.0.2-auto-beta release on IMX8QXP MEK board.

These days we are focusing on the M4 Core booting time(from POW ON to m4 demp app run).

As we tested it always need 170~250ms.

Then we enabled the scfw debug log, it shows the SCU ROM boot time need 150ms!

-------------------------------

Hello from SCU (Build 3014, Commit f0226b37, Mar 2Hello from SCU (Build 3014, Commit f0226b37, Mar 27 2019 14:44:44)

 

SCFW: DDR frequency = 1200000000

ROM boot time  = 154894 usec   <<< Here, does it really mean the SCU PROM loading time ?

SCFW boot time  = 20852 usec

        Banner  = 6 usec

        Init    = 5447 usec

        Config  = 2969 usec

        DDR     = 5797 usec

        SConfig = 196 usec

        Prep    = 4310 usec

*** Debug Monitor ***

--------------------------------

If it's true, is it possible to reduce the ROM boot time in obviously?

In our system design, we hope the M4 can hold the CAN bus msg in < 50ms after power on.

Thanks 

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,569件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tiebing 

>is it possible to reduce the ROM boot time

I am afraid not, since rom sources can not be changed.

In general one can check boot mode settings which may affect speed,

like SCU_ICACHE_DISABLE described inTable 5-3. Boot eFuse Descriptions

i.MX8QXP Reference Manual. Avoid logo and ddr initialization and run code from

internal memories. Also additional boot time optimizations may be provided

based on customer specific needs with NXP Professional Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,569件の閲覧回数
tiebing_guo
Contributor I

Dear Igorpadykov

Thanks for kindly reply at all.

About the Boot eFuse:

Is there any visible result about ROM boot speed improvement after fused some boot eFuse bits?

Can NXP help to give us the best eFuse set for boot speed improve? As you know eFuse is one time writable area, customer has no much opportunity to try find the best set....

About the Avoid logo and ddr initialization and run code from internal memories

This is talking about the SCU FW and M4 core execution, is it right?

According to the standard Boot Flow, during scu rom booting seq, it needs the SECO FW to authentication image containers, it would take some time... is it possible to ignore the image authentication for faster boot, like the early boot flow in SCFW?


Thanks very much~

0 件の賞賛
返信

2,569件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tiebing

one can look at boot optimizations implemented in Android AUTO :

i.MX Software | NXP 

>Can NXP help to give us the best eFuse set for boot speed improve?

I am afraid there will be no significant improvement with fuse boot option.

>it needs the SECO FW to authentication image containers, it would take some time... 

> is it possible to ignore the image authentication for faster boot, like the early boot flow in SCFW?

not, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信