SAIF2 interrupt on iMX233 (WINCE6 R3)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAIF2 interrupt on iMX233 (WINCE6 R3)

982件の閲覧回数
MenM
Contributor I

Hi,

I try to get SAIF2 up and running on a iMX233. I see that the DMA command complete interrupt is set after a DMA transfer, but my thread is not serviced. If I do the same with SAIF1 everything works fine. (SAIF1is using another interrupt number)

anyone ho has ever tried using SAIF2 on an iMX233 or any suggestions to debug the interrupt piece from dma to interrupt controller?

thanks in advance,

Maarten.

タグ(1)
0 件の賞賛
返信
0 返答(返信)