SAI1_MCLK can't output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAI1_MCLK can't output

1,303 Views
kenmeng
Contributor II

HI

Why the SAI1_MCLK Can't output to the Pin.

PinMux: CSI_DATA01,  Mode(ALT6), PAD_CTL (Pull up with 47kohm, SPEED_3_max_200MHz, Fast_Slew_rate)

The other signal of the SAI (include BCLK、FS、DAIN) are all output correctly.

BestRegards!

0 Kudos
Reply
3 Replies

1,134 Views
art
NXP Employee
NXP Employee

SAIx_MCLK is not an output. This is just the optional external master clock input for the SAI module to derive all other clocks (bit clock, frame sync clock) from it. So, nothing should be output on this line.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,134 Views
kenmeng
Contributor II

pastedImage_1.png

Hi Artur,

     This from imx6ul TRM,please check it!

0 Kudos
Reply

1,134 Views
chris_c
Contributor II

Can someone confirm if SAI1_MCLK is an output?  I'm facing the same issue.

0 Kudos
Reply