SAI1_MCLK can't output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SAI1_MCLK can't output

1,371 次查看
kenmeng
Contributor II

HI

Why the SAI1_MCLK Can't output to the Pin.

PinMux: CSI_DATA01,  Mode(ALT6), PAD_CTL (Pull up with 47kohm, SPEED_3_max_200MHz, Fast_Slew_rate)

The other signal of the SAI (include BCLK、FS、DAIN) are all output correctly.

BestRegards!

0 项奖励
回复
3 回复数

1,202 次查看
art
NXP Employee
NXP Employee

SAIx_MCLK is not an output. This is just the optional external master clock input for the SAI module to derive all other clocks (bit clock, frame sync clock) from it. So, nothing should be output on this line.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,202 次查看
kenmeng
Contributor II

pastedImage_1.png

Hi Artur,

     This from imx6ul TRM,please check it!

0 项奖励
回复

1,202 次查看
chris_c
Contributor II

Can someone confirm if SAI1_MCLK is an output?  I'm facing the same issue.

0 项奖励
回复