SAI Codec/DSP mode waveforms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAI Codec/DSP mode waveforms

1,993 Views
apiscozzo
Contributor II

Hi all,

I've been working on a project with the i.MX8 MQ.

The reference manual IMX8MDQLQRM at page 5059 reads:

"The I2S (or I2S) module provides a synchronous audio interface (SAI) that supports fullduplex
serial interfaces with frame synchronization such as I2S, AC97, TDM, and
codec/DSP interfaces"

I found this one (link). At page 4, it explains exactly how the SAI  works in that mode but the document is about another microprocessor.

Question:
Can I assume that the SAI works in the same way in any NXP silicon where it's implemented?
Is there any NXP official document which shows and describes the wave-forms of this specific operation mode for the iMX8MQ?

Thanks and kind regards,

Alessandro

0 Kudos
Reply
1 Reply

1,914 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

We do not suggest to see other documentation that is from another completely different chip. What I suggest you is to see the i.MX8MQ reference manual on the SAI part of the product. There you could find everything that is needed to understand how the SAI peripheral works in the i.MX8MQ.

Please see section13.8 page 5501 of the i.MX8MQ reference manual.

Best regards,

Diego.

0 Kudos
Reply