SABRE Record Camera Video

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE Record Camera Video

2,152件の閲覧回数
amassa
Contributor II

Hi,

I was wondering if there was a way to record the camera video input to storage (SD card) on the SABRE board. I am able to get the camera output to the display (SDP) and have streamed it, but I would also like to record the camera input to the SD card.

Any help is greatly appreciated.

Thanks.

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,787件の閲覧回数
amassa
Contributor II

Thanks for the response. I am looking for an example if someone has stored a video stream on the SD card on the SABRE board.

Thanks.

0 件の賞賛
返信

1,787件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may try using "tee" or just to run several gstreamer pipelines as different Linux tasks.

But performance may be an issue in such cases.

GStreamer i.MX6 Pipelines


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信