SABRE Record Camera Video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE Record Camera Video

2,139 Views
amassa
Contributor II

Hi,

I was wondering if there was a way to record the camera video input to storage (SD card) on the SABRE board. I am able to get the camera output to the display (SDP) and have streamed it, but I would also like to record the camera input to the SD card.

Any help is greatly appreciated.

Thanks.

Labels (3)
0 Kudos
Reply
2 Replies

1,774 Views
amassa
Contributor II

Thanks for the response. I am looking for an example if someone has stored a video stream on the SD card on the SABRE board.

Thanks.

0 Kudos
Reply

1,774 Views
Yuri
NXP Employee
NXP Employee

You may try using "tee" or just to run several gstreamer pipelines as different Linux tasks.

But performance may be an issue in such cases.

GStreamer i.MX6 Pipelines


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply