[S32R294] SPT enable issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32R294] SPT enable issue

2,486件の閲覧回数
GaryKuo
Contributor I

Hi Sir,

I' m testing with S32R294 EVB board (v1.1).

When I tried to initialize SPT, I got `RSDK_SPT_RET_ERR_HW_RST` error state.

This is because pSptRegs->CS_STATUS3.B.PROC_STATE is 0, so that  CheckSptRst() in SptConfigHw() return RSDK_SPT_RET_ERR_HW_RST.

But when I try RSDK_offline_example, I found `pSptRegs->CS_STATUS3.B.PROC_STATE` is "1" in  SptConfigHw() and can success pass initial process.

Is there anything I should enable before SPT is launched?

Can you suggest me how to solve this issue?

 

Thank you,

Gary

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,424件の閲覧回数
GaryKuo
Contributor I

Hi,

I've solved this issue, thank you.

Gary

0 件の賞賛
返信

2,431件の閲覧回数
b41937
NXP Employee
NXP Employee

Hi,

Can you provide some context in which this error occurs? It would help if we can reproduce the issue but my understanding is that the provided examples work. 

0 件の賞賛
返信