Running software without an underlying OS (Linux, Windows, Android, ...)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running software without an underlying OS (Linux, Windows, Android, ...)

3,665件の閲覧回数
jimpanse
Contributor II

Hey folks,

i want to run some code directly (without an OS) on my i.MX53 QSB. Can you help me with that?

Is there any documentation available?

Thanks!!

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,460件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Jimpanse,

You can run standalone code through JTAG. Chapter 9 of the users guide says how to do it. You can find the users guide in the following link:

http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf?fpsp=1&WT_TYPE=UsersGuides&WT_VENDO...

About the code, you can write it in Eclipse, which is a freeware you can download from www.eclipse.org. After you finish the code, you can also compile it as a binary and flash it, this way you don't need JTAG.

Best regards.

Jorge.

3,460件の閲覧回数
jimpanse
Contributor II

Hey Jorge,

can you explain these steps a bit more detailed?

About the code, you can write it in Eclipse, which is a freeware you can download from www.eclipse.org. After you finish the code, you can also compile it as a binary and flash it, this way you don't need JTAG.

Which toolchain can I use? The CodeSourcery Lite Toolchain?

What do you mean by flashing without JTAG? Flashing the binary to the SD-Card? Which tool can I use?

Thanks in advance!

0 件の賞賛
返信

3,460件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

There is a test code (without any OS) for i.MX53QSB called IMX53_QSB_OBDS .  You can download it from the i.MX53QSB web page.

3,460件の閲覧回数
jimpanse
Contributor II

Thank you very much. I've searched for something like this! :smileyhappy:

0 件の賞賛
返信