Run boot.img from usb in u-boot time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Run boot.img from usb in u-boot time

1,384 次查看
kulbhushankashy
Contributor I

Hi,

I am using IMX6 sabre solo based board and I want to load boot.img form usb when i am at u-boot prompt.

what to do for load boot.img at u-boot prompt where boot.img is in usb?

Regards,

Kulbhushan

0 项奖励
回复
1 回复

979 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Kulbhushan,

Please note that there are two Linux releases: official Freescale BSPs (which we [TIC] support) and Community BSPs (which we do not support, it is supported through Community or Yocto mailing list:  https://lists.yoctoproject.org/listinfo/meta-freescale).

Differences are described on below link

http://freescale.github.io/doc/release-notes/1.8/

Seems uboot from Community BSPs releases supports USB in U-Boot. You could post your question on Yocto mailing list for more details.

You could also refer to the following threads, which discus similar issues:

https://community.freescale.com/thread/376236

https://community.freescale.com/thread/311585


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复