Run Matter Example - iMX8ULP-EVK9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run Matter Example - iMX8ULP-EVK9

1,471 Views
dhruvinrajpura
Contributor III

Hello,

I am using imx8ulp evk9 and esp32, I did yocto build for imx8ulp-evk9 and built imx-image-core,
I want to run basic matter ble example in that I have esp32 as well with me, from 8ulp side what kind of setup I need to have and what will be commands and all?

Labels (1)
0 Kudos
Reply
4 Replies

1,436 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using? How the ESP32 connect to the i.MX8ULP EVK board?

0 Kudos
Reply

1,432 Views
dhruvinrajpura
Contributor III

I am using 6.6-scarthgap BSP, and 'll not connect ESP32 with 8ulp, I will start matter on esp32 and ulp both and will communicate over wifi.

What I need to setup on 8ulp side for that?

0 Kudos
Reply

1,406 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can refer to our I.MX Matterand README

GitHub - NXP/matter at v1.4-branch-nxp_imx_2024_q4

0 Kudos
Reply

1,449 Views
dhruvinrajpura
Contributor III

Can anyone make some comment on this?

0 Kudos
Reply