Rotate screen with imx-image-desktop on i.MX8MQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rotate screen with imx-image-desktop on i.MX8MQ

942件の閲覧回数
Derek0902
Contributor II

Hi,

I'm trying gnome desktop on imx8mq and I want to use xrandr to rotate screen. 

When I use this command, there is no effective on screen.

 

xrandr -o right

 

 

Another question is that I found the connector is XWAYLAND but is not DP-1. Because my panel is DP connector.

PXL_20240415_085856371.jpg

Regards,

Derek Lin

0 件の賞賛
返信
2 返答(返信)

914件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you are using yocto, the MX8MQ does not use X11, it use wayland.

Regards

0 件の賞賛
返信

912件の閲覧回数
Derek0902
Contributor II

Hi @Bio_TICFSL ,

How can I rotate the gnome desktop by using command ?

Another way is auto rotate of gnome-shell-extensions.

I follow this Github and add this extensions:gnome-shell-extension-screen-autorotate

But the gnome version is gnome 42.9 so it need to modify the code to support gnome 42. You can follow it : Add support for GNOME 42 

I have added this extension and the auto-rotate icon appear on screen.

64037_0.jpg

64047.jpg

The iio device is work when I use monitor-sensor to check it.

64036_0.jpg

But the screen can not rotate and there is no effective on screen.

Has anyone encountered this problem?

 

Thanks & Regards,

Derek Lin 

0 件の賞賛
返信