Resizing the video frame using mfw_v4lsink plugin is not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Resizing the video frame using mfw_v4lsink plugin is not working

1,480 次查看
ashutosh10509
Contributor I

I am trying to resize the video frame using mfw_v4lsink plugin but it is not working. This problem is coming with mfw_v4lsink plugin installed in gst-fsl-plugins-3.0.11 package.

When i am trying set video frame size at the start of the pipeline , it's not working but when i do the same thing after 1 second of playback , it's working.

During debugging i didn't found the above problem with mw_4lsink plugin installed in gst-fsl-plugins-3.0.7 package. When i looked into the code of version 3.0.11 and 3.0.7 , there was a lot of changes in mfw_v4lsink plugins , so i was not able to figure it out what causing the problem.

Test code :

#include <gst/gst.h>

#include <gst/gstcaps.h>

#include <stdio.h>

#include <string.h>

#include <stdlib.h>

typedef struct App {

    GstElement *pipeline;

    GstElement *source;

    GstElement *demuxer;

    GstElement *audioDecoder;

    GstElement *videoDecoder;

    GstElement *audioQueue;

    GstElement *videoQueue;

    GstElement *audioResampler;

    GstElement *videoScaler;

    GstElement *audioSink;

    GstElement *videoSink;

    GstElement *videoCapsFilter;

    GMainLoop *loop;

}App;

static void

on_pad_added (GstElement *element,

              GstPad     *pad,

              gpointer    data) {

    App *app = (App *) data;

    GstCaps *caps = gst_pad_get_caps(pad);

    GstStructure *structure = gst_caps_get_structure(caps, 0);

    if(g_strrstr(gst_structure_get_name(structure), "video")) {

        GstPad *videoQueuePad = gst_element_get_pad(app->videoQueue,"sink");

        gst_pad_link(pad,videoQueuePad);

        gst_element_link(app->videoQueue,app->videoDecoder);

        gst_element_link(app->videoDecoder,app->videoSink);

       // gst_element_link(app->videoScaler,app->videoSink);

        gst_object_unref(videoQueuePad);

        gst_caps_unref(caps);

    }

    if(g_strrstr(gst_structure_get_name(structure), "audio")) {

        GstPad *audioQueuePad = gst_element_get_pad(app->audioQueue,"sink");

        gst_pad_link(pad,audioQueuePad);

        gst_element_link(app->audioQueue,app->audioDecoder);

        gst_element_link(app->audioDecoder,app->audioResampler);

        GstCaps *capsFilter = gst_caps_new_simple ("audio/x-raw-int",

                                            "rate", G_TYPE_INT,44100,

                                            "channels", G_TYPE_INT,2,

                                            "depth", G_TYPE_INT,16,

                                            "width", G_TYPE_INT,16,

                                            NULL);

        gst_element_link_filtered(app->audioResampler,app->audioSink,capsFilter);

        gst_caps_unref(capsFilter);

        gst_object_unref(audioQueuePad);

    }

    gst_object_unref (caps);

}

static gboolean

timeout_cb (gpointer user_data) {

    App *app = (App*)user_data;

    g_object_set (G_OBJECT (app->videoSink), "setpara", 1, NULL);

    g_object_set (G_OBJECT (app->videoSink), "disp-width", 400 ,NULL);

    g_object_set (G_OBJECT (app->videoSink), "disp-height", 240, NULL);

    return TRUE;

}

static gboolean

bus_cb (GstBus * bus, GstMessage * msg, gpointer user_data)

{

  App *app  = (App*)user_data;

  switch (GST_MESSAGE_TYPE (msg)) {

    case GST_MESSAGE_ERROR:{

      GError *err = NULL;

      gchar *dbg;

      gst_message_parse_error (msg, &err, &dbg);

      gst_object_default_error (msg->src, err, dbg);

      g_error_free (err);

      g_free (dbg);

      g_main_loop_quit (app->loop);

      break;

    }

    default:

      break;

  }

  return TRUE;

}

int

main (int   argc,

      char *argv[])

{

    App app;

    GstBus *bus;

    guint bus_watch_id;

    /* Initialisation */

    gst_init (&argc, &argv);

    app.loop = g_main_loop_new (NULL, FALSE);

    /* Check input arguments */

    if (argc != 2) {

        printf("Usage: %s <filename>\n", argv[0]);

        return -1;

    }

    /* Create gstreamer elements */

    app.pipeline = gst_pipeline_new ("audio-player");

    app.source   = gst_element_factory_make ("filesrc","source");

    app.demuxer  = gst_element_factory_make ("tsdemux","demuxer");

    app.audioQueue = gst_element_factory_make ("queue","audio-queue");

    app.videoQueue = gst_element_factory_make ("queue","video-queue");

    app.audioDecoder  = gst_element_factory_make ("faad","audio-decoder");

    app.videoDecoder  = gst_element_factory_make ("vpudec","video-decoder");

    app.audioResampler  = gst_element_factory_make ("audioresample", "audio-resampler");

    app.videoScaler = gst_element_factory_make ("videoscale", "video-scaler");

    app.audioSink = gst_element_factory_make ("alsasink", "audio-sink");

    app.videoSink = gst_element_factory_make ("mfw_v4lsink", "video-sink");

    app.videoCapsFilter = gst_element_factory_make ("capsfilter", "caps-filter");

    if (!app.pipeline || !app.source || !app.demuxer || !app.audioDecoder

          || !app.videoDecoder || !app.audioResampler || !app.videoScaler

          || !app.audioSink || !app.videoSink || !app.audioQueue

           || !app.videoQueue) {

        printf("One element could not be created. Exiting.\n");

        return -1;

    }

    /* Set up the pipeline */

    /* we set the input filename to the source element */

    g_object_set (G_OBJECT (app.source), "location", argv[1], NULL);

    g_object_set (G_OBJECT (app.source), "do-timestamp", TRUE, NULL);

    g_object_set (G_OBJECT (app.videoSink), "sync", FALSE, NULL);

    g_object_set (G_OBJECT (app.videoSink), "disp-width", 400 ,NULL);

    g_object_set (G_OBJECT (app.videoSink), "disp-height", 240, NULL);

    g_object_set (G_OBJECT (app.videoSink), "async", 0, NULL);

    /* we add a message handler */

    bus = gst_pipeline_get_bus (GST_PIPELINE (app.pipeline));

    bus_watch_id = gst_bus_add_watch (bus, bus_cb,&app);

    gst_object_unref (bus);

    /* we add all elements into the pipeline */

    gst_bin_add_many (GST_BIN (app.pipeline),

                    app.source,

                    app.demuxer,

                    app.audioQueue,

                    app.videoQueue,

                    app.audioDecoder,

                    app.videoDecoder,

                    app.audioResampler,

                    app.videoScaler,

                    app.audioSink,

                    app.videoSink,

                    app.videoCapsFilter,

                    NULL);

    /* we link the elements together */

    gst_element_link (app.source,app.demuxer);

    g_signal_connect (app.demuxer, "pad-added", G_CALLBACK (on_pad_added),&app);

    /* Set the pipeline to "playing" state*/

    printf ("Now playing: %s\n", argv[1]);

    gst_element_set_state (app.pipeline, GST_STATE_PLAYING);

    g_timeout_add_seconds (2, timeout_cb, &app);

    /* Iterate */

    g_main_loop_run (app.loop);

    /* Out of the main loop, clean up nicely */

    printf ("Returned, stopping playback\n");

    gst_element_set_state (app.pipeline, GST_STATE_NULL);

    printf ("Deleting pipeline\n");

    gst_object_unref (GST_OBJECT (app.pipeline));

    g_source_remove (bus_watch_id);

    g_main_loop_unref (app.loop);

  return 0;

}

0 项奖励
回复
1 回复

1,151 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Ashutosh,

Have you try the following pipeline:

gst-launch v4l2src device=/dev/video0 ! mfw_v4lsink device=/dev/video18 disp-width=1920 disp-height=1080

See the comments on the following Link:

Re: How to resize the video in gstreamer-1.0?

0 项奖励
回复