Request for Prebuilt Yocto Images for i.MX6SXSABRE-SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Prebuilt Yocto Images for i.MX6SXSABRE-SD

753 Views
Ajay333
Contributor I

Hi,

I'm currently working on bringing up the i.MX6SX SABRE-SD (MACHINE: imx6sxsabresd) board and would like to request the latest available prebuilt images for initial testing and validation.

If available, could you kindly share the following:
- core-image-minimal or core-image-base prebuilt .wic or .sdcard images
- Corresponding u-boot.imx
- Matching DTB and kernel (zImage/Image) files

Looking forward to your support.

Labels (1)
0 Kudos
Reply
4 Replies

656 Views
Harvey021
NXP TechSupport
NXP TechSupport

Reply back to you from your private message 

 

Regards

Harvey

0 Kudos
Reply

719 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

prebuild images can be downloaded from embedded-software for different releases.

The one MX6QDLSOLOX is the latest version, and it is full image. 

For core-image-minimal or core-image-base, you need to build it as reference - USERS_GUIDE and imx-manifest 

 

Regards

Harvey

0 Kudos
Reply

688 Views
Ajay333
Contributor I

Hi

The other method we have tried flashing the uboot, zimage, dtb and rfs to the corresponding partition still the issue persist.

0 Kudos
Reply

691 Views
Ajay333
Contributor I

Hi

We have tried flashing the latest full image MX6QDLSOLOX (imx-image-full-imx6qpdlsolox.wic) using balena etcher, even though the mode of boot is through SD card, still the device is not getting booted, we have listed out the usb devices, only the blank detetction of the device is notified.Screenshot from 2025-04-28 11-35-20.png

0 Kudos
Reply