Remapping vector table in the iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Remapping vector table in the iMX6

2,159 Views
ogj
Contributor IV

I'm having an issue/misunderstanding on remapping the vector table for the A9 core (iMX6 Quad) in a bare metal (flat mapped) application. I assumed I could create a vector table in some arbitrary location in RAM, load that location into the vbar register:

ldr r0, =vector_tbl
mcr p15, 0, r0, c12, c0, 0 //write VBAR register

and when an interrupt occurred (via the gic/IRQ), control would pass to the IRQ handler. This isn't happening. Control actually passes to the svc handler with the cpu in IRQ mode. I'm pretty sure this is a result of not remapping the vector table correctly. Any guidance on this?

Labels (1)
0 Kudos
Reply
2 Replies

2,155 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The Remapping vector table code in start.S/vectors.S is not written by nxp. You should post this issue in linux kernel site.And this start code shouldn't have errors.

0 Kudos
Reply

2,142 Views
ogj
Contributor IV

Got the answer from ARM. The vector table must be on a 32-byte boundary.

0 Kudos
Reply