Remap secure bootloader flow chart seems wrong

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Remap secure bootloader flow chart seems wrong

Jump to solution
7,039 Views
pm_2552
Contributor III

Hello,

It appears that the Remap flow chart for SBL has some typos and is not the updated one. Can you please provide the correct flow chart?

 

0 Kudos
Reply
1 Solution
6,942 Views
pm_2552
Contributor III

Remap_signature_verification.png

Please check the highlighted part in the above flow chart. I have marked all blocks where Remap is enabled with "++" and where Remap is disabled to "--"
The enable Remap block in the above flow should be before verification and that is indeed the case in the SBL code.

View solution in original post

0 Kudos
Reply
4 Replies
6,943 Views
pm_2552
Contributor III

Remap_signature_verification.png

Please check the highlighted part in the above flow chart. I have marked all blocks where Remap is enabled with "++" and where Remap is disabled to "--"
The enable Remap block in the above flow should be before verification and that is indeed the case in the SBL code.

0 Kudos
Reply
6,997 Views
pm_2552
Contributor III

@kerry zhou Can you please help?

7,006 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @pm_2552 ,

I hope you're doing well!

What device are you using?

Thank you.

Best regards,
Hector.

0 Kudos
Reply
6,998 Views
pm_2552
Contributor III

Hello I am using RT1060 and this are the docs I am referring to: AN13460

0 Kudos
Reply