Relaxing LPDDR4 timings for high temperature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Relaxing LPDDR4 timings for high temperature

ソリューションへジャンプ
3,322件の閲覧回数
frank_vanhooft
Contributor III

We're using an iMX8-mini with a single LPDDR4 x32 device. We're working on qualifying second and third source LPDDR4 chips, and having a little difficulty with some parts when running memtester at high temperature (75 C ambient or higher). We're using industrial-temp or automotive-temp parts rated for 1600 speed grade. We run the imx8 DDR interface at 1500 (as configured in the RPA spreadsheet). At high temps we still see the occasional memtester error with certain RAM chips.

In the RPA spreadsheet, I've selected "option 2" for the LPDDR4 MR4 manual de-rate workaround.

I'm looking for suggestions regarding which parameters I might change in the RPA spreadsheet to accommodate looser timings for the RAM, to help it at the higher temperatures.

Thanks.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
3,269件の閲覧回数
frank_vanhooft
Contributor III

I'm going to close this. I contacted an NXP guru, who pointed me to this:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRA...

That gave us the pointers we needed to move forward. We have the part working at high temps now. Thanks.

元の投稿で解決策を見る

4 返答(返信)
3,270件の閲覧回数
frank_vanhooft
Contributor III

I'm going to close this. I contacted an NXP guru, who pointed me to this:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRA...

That gave us the pointers we needed to move forward. We have the part working at high temps now. Thanks.

3,296件の閲覧回数
frank_vanhooft
Contributor III

-40 to +105C

Alliance AS4C256M32MD4-062BAN

0 件の賞賛
返信
3,275件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

At high temps we still see the occasional memtester error with certain RAM chips.

Could you share the full log  to us?

0 件の賞賛
返信
3,302件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

How about the temperature range of the DDR you are using?

0 件の賞賛
返信