Relation between PLL Freq and SSI's sys clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Relation between PLL Freq and SSI's sys clock

ソリューションへジャンプ
3,536件の閲覧回数
yehudastern
Contributor II

Hi,

1.  The relation between PLL Freq and SSI's sys clock is given by SSIDIV (in CCM).   Is that the product of SSIx_clk_pred and SSIx_clk_podf ?

     (I set PLL4 frequency to 688.128 MHz and SSIDIV to 56, and would expect SSI's sys clock to be 12.288 MHz).

2.  mxc_wm8962_init() function in board-mx6q_sabresd.c includes the following code:

     rate = clk_round_rate(clko, 24000000);

     clk_set_rate(clko, rate);

     wm8962_data.sysclk = rate;

     But when I read wm8962_data.sysclk, I receive 86.016 MHz, which is 7 times the expected value.

     What's the purpose of this code?  Can it simply be replaced with:   rate = clk_set_rate(clko, 12288000);  ?

3.  When measuring the Serial BIT clock with a scope, I always get 1.4112 MHz instead of 1.536 MHz.  

      Any idea why?  (is that the default value given by the driver?)

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
3,293件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yehuda

you can output some clocks for check using

CCM_CCOSR register

~igor

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,293件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yehuda

1. I believe you are right, in particular Figure 61-22. SSI Transmit Clock Generator Block Diagram

i.MX6DQ RM http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

shows origin of SSI's sys clock

2. please look at linux clock framework description on web resources, like

http://elinux.org/images/b/b8/Elc2013_Clement.pdf

3. seems one needs to reprogram pll, as function like clk_round_rate()

just chooses frequency close to necessary

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,293件の閲覧回数
yehudastern
Contributor II

Hi Igor,

1.  Figure 61-22 (SSI Transmit Clock Generator Block Diagram in i.MX6DQ RM) shows SSI's sys clock as the input clock, but doesn't show its origin.

     I need to verify whether SSIDIV in Table 61-7 is the product of SSIx_clk_pred and SSIx_clk_podf (taken from CCM_CS1CDR & CCM_CS1CDR registers).

2.  Is there any way to read the real SSI's sys clock inside i.MX6 ?

3.  Please correct me if I'm wrong: 

     - Since Serial BIT clock measured with a scope is an input to the codec, and since mxc_wm8962_init() function only deals with the codecs internal PLL, the

       Serial BIT clock cannot be influenced by this function, and can only be influenced by the contents of the following registers (i.e. no other registers are involved): 

       CCM_ANALOG_PLL_AUDIO,     (BTW, what's the difference between this register and CCM_ANALOG_PLL_AUDIO_SET / CLR ?)

       CCM_ANALOG_PLL_AUDIO_NUM,

       CCM_ANALOG_PLL_AUDIO_DENOM,

       CCM_CS1CDR / CCM_CS2CDR

       CCM_CSCMR1,

       SSI1_STCCR / SSI2_STCCR / SSI2_STCCR.

BR

Yehuda

      

0 件の賞賛
返信
3,294件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yehuda

you can output some clocks for check using

CCM_CCOSR register

~igor

0 件の賞賛
返信
3,293件の閲覧回数
yehudastern
Contributor II

Hi Igor,

Thanks.  It seems that SSI's sys clock can also be output to the network clock as illustrated on figure 61-22.

I would appreciate it if you can also advise regarding questions 1 & 3.

Thanks.

0 件の賞賛
返信