Regarding i.MX6 Linux BSP for year 2038 problem.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding i.MX6 Linux BSP for year 2038 problem.

Jump to solution
2,781 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Linux BSP.

You know Linux kernel 3.14 has year 2038 problem.

Would you let me know whether has NXP release a patch for BSP or not?

If not, would you let me know how fix year 2038 problem?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1 Solution
2,399 Views
b36401
NXP Employee
NXP Employee

Hello,

Actually we migrate the kernels every year.

So we will wait for this issue to be completely solved in future Linux kernel and then we will use this kernel.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,154 Views
MichaelChristian
Contributor I

This topic is now 6 years old. I am using BSP L4.1.15_2.0.0 which has the year 2038 problem. Has a current BSP addressed the 2038 problem yet, and if not what are the plans in this area?

0 Kudos
Reply
2,400 Views
b36401
NXP Employee
NXP Employee

Hello,

Actually we migrate the kernels every year.

So we will wait for this issue to be completely solved in future Linux kernel and then we will use this kernel.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply