Regarding i.MX6 Linux BSP for year 2038 problem.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding i.MX6 Linux BSP for year 2038 problem.

ソリューションへジャンプ
3,744件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Linux BSP.

You know Linux kernel 3.14 has year 2038 problem.

Would you let me know whether has NXP release a patch for BSP or not?

If not, would you let me know how fix year 2038 problem?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1 解決策
3,362件の閲覧回数
b36401
NXP Employee
NXP Employee

Hello,

Actually we migrate the kernels every year.

So we will wait for this issue to be completely solved in future Linux kernel and then we will use this kernel.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,117件の閲覧回数
MichaelChristian
Contributor I

This topic is now 6 years old. I am using BSP L4.1.15_2.0.0 which has the year 2038 problem. Has a current BSP addressed the 2038 problem yet, and if not what are the plans in this area?

0 件の賞賛
返信
3,363件の閲覧回数
b36401
NXP Employee
NXP Employee

Hello,

Actually we migrate the kernels every year.

So we will wait for this issue to be completely solved in future Linux kernel and then we will use this kernel.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信