Regarding PCB design with IMX6POP.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding PCB design with IMX6POP.

1,699 次查看
tomohisa_sakamo
Senior Contributor III

We consider PCB design with IMX6POP(IMX6DQCPOPEC).
We need below answers asap.

Section 3.18 of the HW Design Guide indicates that when using a POP product,
 the impedance of the VIA of the build-up board is
It becomes dominant, it can not be satisfied by becoming a value about three times the standard.
So please let us ask the question below.

1. Below, We  think that it is regulation in the simulation of reference board which is not POP item
     Could you please tell us the criteria for POP items?

2. If the following can not be fulfilled, please tell us if there is any other solution.

■ Hardware Development Guide for i.MX 6QuadPlus, 6Quad, 6DualPlus, 6Dual, 6DualLite, 6Solo Families of Applications Processors
        IMX6DQ6SDLHDG Rev. 2 10/2016

 P.68
3.18 Guideline for power net electrical performance
              The graph is provided as impedance guidance for the various power nets relative to ground.
              NXP recommends that a user’s board be at or below the impedances curves shown. For example,
              consider the 100 MHz point on the VDD_ARM_CAP curve at 0.065 ohms. User layouts at 100 MHz
              should have impedance from VDD_ARM_CAP to ground of 0.065 ohms or less.

标签 (2)
0 项奖励
回复
2 回复数

1,583 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Please create request for further discussion.

https://community.nxp.com/docs/DOC-329745 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复

1,583 次查看
vijaikumar
Contributor III

Hi Tomohisa,

                      If you are willing to go for ready-to-deploy iMX6QPOP based SoM modules for your end design , please have a look at https://www.mistralsolutions.com/product-engineering-services/products/vise-board/ 

Thanks,

Vijai

0 项奖励
回复