アクセスしようとしているメッセージは完全に削除されました。
How to connect USB type C to USB type B using HSIC without USB cable? Need a schematic diagram or interchip USB IC Details for to make the connection
解決済! 解決策の投稿を見る。
Hi suracece27
for usage one can look at i.MX7ULP EVK, it has hsic connectors
Specification :
https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/23638/1/High Speed Inter-Chip_1_0 final.pdf
Best regardsigor
元の投稿で解決策を見る
Dear Igorpady Kav,
I have https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-8quadmax-m...
I need to connect the same board with another custom made board which is having Cypress USB Controller https://www.cypress.com/file/140296/download
I need to connect both the boards using HSIC without having any USB receptacle.
I hope it's clear.
Need to connect both the boards without a USB connector with HSIC schematic reference diagram I am looking.
Thanks and Regards
Suresh
Thanks a lot for your prompt reply. I will check and update the same..