Regarding Interchip USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Regarding Interchip USB

跳至解决方案
2,666 次查看
suracece27
Contributor I

How to connect USB type C to USB type B using HSIC without USB cable? Need a schematic diagram or interchip USB IC Details for to make the connection

0 项奖励
回复
1 解答
2,661 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  suracece27

 

for usage one can look at i.MX7ULP EVK,  it has hsic connectors

MCIMX7ULP-EVK Design Files

Specification :

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/23638/1/High Speed Inter-Chip_1_0 final.pdf

 

Best regards
igor

在原帖中查看解决方案

3 回复数
2,644 次查看
suracece27
Contributor I

Dear Igorpady Kav,

I have  https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-8quadmax-m...

I need to connect the same board with another custom made board which is having Cypress USB Controller https://www.cypress.com/file/140296/download

I need to connect both the boards using HSIC without having any USB receptacle.

I hope it's clear.

Need to connect both the boards without a USB connector with HSIC schematic reference diagram I am looking.

Thanks and Regards

Suresh

 

0 项奖励
回复
2,662 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  suracece27

 

for usage one can look at i.MX7ULP EVK,  it has hsic connectors

MCIMX7ULP-EVK Design Files

Specification :

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/23638/1/High Speed Inter-Chip_1_0 final.pdf

 

Best regards
igor

2,654 次查看
suracece27
Contributor I

Thanks a lot for your prompt reply. I will check and update the same..

0 项奖励
回复