Regarding FlexSPI AHB Memory access Range

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Regarding FlexSPI AHB Memory access Range

跳至解决方案
2,295 次查看
GopiKrishna
Contributor II

Hi,

We are trying to access two MT25QL(each 256MB in size) serial flash devices in Parallel flash mode using Flexspi on PIMX8QM5AVUDDAA-PR. We are able to read from both flashes using AHB command mode. we had an observation that by using the AHB mode we are able to access only up to 0x0 to 0x10000000(256MB). We had a requirement to access it up to 0x0 to 0x20000000(512MB) for faster read access. 

is there any way to increase the range of AHB memory access?

we are using the AMBA base address as 0x08000000 is there any register configuration to change this base address and AHB memory map size?

0 项奖励
回复
1 解答
2,258 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @GopiKrishna!

On i.MX8QM, AHB mapping of flexspi0+Other is 320MB, in which, I think 256MB is for FlexSPI0 mapping.

Chavira_0-1688430020687.png

 

So with flexspi0, I'm afraid the memory range can only be 256MB.

But it seems the AHB mapping of flexspi1+Other is 1GB.

Best Regards.

Chavira

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,240 次查看
GopiKrishna
Contributor II

Hi @Chavira 

  Thank you for the clarification. The information that you shared is helpful for us.

2,259 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @GopiKrishna!

On i.MX8QM, AHB mapping of flexspi0+Other is 320MB, in which, I think 256MB is for FlexSPI0 mapping.

Chavira_0-1688430020687.png

 

So with flexspi0, I'm afraid the memory range can only be 256MB.

But it seems the AHB mapping of flexspi1+Other is 1GB.

Best Regards.

Chavira

0 项奖励
回复