IMX8MP Power Group Conflict

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MP Power Group Conflict

跳至解决方案
4,884 次查看
tomo
Contributor II

Hi all,

I'm designing a custom board with iMX8MP and PCA9450C.
NVCC_GPIO is connected to the 3.3V power supply and NVCC_SD2 is his LDO5 output of the PCA9450C.
My circuit has a USDHC2 interface that I use for an SD card and the VSEL signal is connected from GPIO1_IO04 to the PCA9450C's SD_VSEL pin.
Are there any issues with this configuration?
In Config Tools for i.MX v13, when I set NVCC_SD2=1.8V and NVCC_GPIO1=3.3V, I get a warning that the voltages are in conflict, so I would like to ask you just in case.
I am attaching an image of the warning message.

Best regards,

tomo

 

0 项奖励
回复
1 解答
4,840 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Yes, that setting is also correct.

Thanks & Regards,
Ritesh M Patel

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,868 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @tomo,

I hope you are doing well.

uSDHC2_VSEL is connected to GPIO1_IO4. However, the NVCC_SD2 voltage is set to 1.8V and the NVCC_GPIO1 voltage is set to 3.3V. Since uSDHC2 is referenced to NVCC_SD2 power rail, there would be a warning of voltage conflict.

If you change the NVCC_GPIO1 voltage to 1.8V, the warning would vanish. Please check.

I hope it helps.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复
4,864 次查看
tomo
Contributor II

Hi riteshmpatel,

Thank you for your reply.
I followed your suggestion and the warning disappeared.
Conversely, when I set NVCC_SD2 to 3.3V, the warning disappeared as well.
Is this setting also correct?

Best regards,

tomo

0 项奖励
回复
4,841 次查看
riteshmpatel
NXP TechSupport
NXP TechSupport

Yes, that setting is also correct.

Thanks & Regards,
Ritesh M Patel

0 项奖励
回复