Reg: Compiling LTIB_Uboot error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reg: Compiling LTIB_Uboot error

跳至解决方案
1,897 次查看
vishvapathi
Contributor V

./ltib -m prep -p u-boot

Installing host support packages.

This only needs to be done once per host, but may take up to

an hour to complete ...

If an error occurs, a log file with the full output may be found in:

/home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/host_config.log

Exiting on error or interrupt

Please see >> /home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/host_config.log for details

cat /home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/host_config.log

Updating lpp from local packages

+ cp -dp /home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/pkgs/u-boot-2009.08 /opt/freescale/pkgs/u-boot-2009.08

cp: omitting directory `/home/vishva/Desktop/L3.0.35_4.0.0_130424_source/yes/ltib/pkgs/u-boot-2009.08'

Died at ./ltib line 2518.

traceback:

main::check_dirs:2518

  main::host_checks:1438

   main:554

how to solve this issue??



标签 (2)
0 项奖励
回复
1 解答
1,692 次查看
jimmychan
NXP TechSupport
NXP TechSupport

After installed the LTIB, please run ./ltib first.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,693 次查看
jimmychan
NXP TechSupport
NXP TechSupport

After installed the LTIB, please run ./ltib first.

0 项奖励
回复