Please look at my comments below.
1.
> Is that means for each DI, the sum of the connected two monitor's timing's pixel clocks can not be larger than 240M ?
Basically - yes. Let me remind MP/sec relates to Pixels / sec, so it is the same as display frequency, when
single clock is needed per pixel.
2.
> For example, we can connected four monitors with mode 1280x1024@60 to the SOC, because the pixel clock
> of 1280x1024@60 is 108M, and two of them are 216M, which is smaller than 240M. In this case, the four monitors
> can work well simultaneously, which is as shown on the figure in my last mail.
> Am I right???
Yes, but again, please do not forgot, that these rates refer only to screen refresh, gated by the capabilities of the
display port. A full use case typically includes additional activities.